Technical FAQs

Ask a Question

Use of BTS with stacked Trace Series inverter chargers

When two Trace Series inverter chargers are stacked in series, only one Battery Temp Sensor is required. The two units will share the battery temperature reading.

Was this helpful?
What can we do to improve the information ?