Technical FAQs

Ask a Question

Where can I source copper cable up to 750 MCM?

You may source copper cable from 6 gauge to 750 MCM size through http://www.cobrawire.com/alternative/solar.php.  As at September 30, 2008, Cobra takes credit card orders and ships anywhere in the US, and they will cut to length. They also supply lugs, but do not attach them to the cabling, so customers must do that upon receipt of their order.  PLEASE measure your cabling requirements carefully and factor in any of the installation requirements for bends and turns, as the largest cable sizes are not flexible.


 


This information is supplied for customer convenience and does not constitute an endorsement of Cobra Wire for end user customers.  Full disclosure: Xantrex purchases from Cobra Wire.

Was this helpful?
What can we do to improve the information ?