Technical FAQs

Ask a Question

Communication Gateway - What pins are what on the RS485 (Modbus) Terminal Block? (eg. Rx+, Rx-, Tx+ and correct orientation)

Pin 1 - 15V input
Pin 2 - Ground
Pin 3 - RS485 A
Pin 4 - RS485 B
 
RS485 is a bidirectional differential bus so there is no transmit and receive. Pin 1 is on the right when looking at the connector. See attached diagram.
 
Was this helpful?
What can we do to improve the information ?