Technical FAQs

Ask a Question

Identify 865-1057 Network Power Supply and 809-0903 Network Tee

These two parts look almost identical externally. In fact the 865-1057 uses the same plastic enclosure. See the attached picture.
The 809-0903 is a Xanbus network Tee and the 865-1057 is a Xanbus Network Power Supply (12VDC@1.5A). They are related because they both may be used in Xanbus network systems. The Tee (809-0903) is rarely used because 99.9% of people install daisy chain networks which do not require the Tee. It is tailored towards the RS/MS inverters, but it is still Xanbus, the network gets installed identically and is a smaller document than the XW installation guide.
The 865-1057 is designed to power a Gateway, but can also be used in any application where there are no network power supplies (XW Inverter/Charger). If a customer wants to use and XW MPPT controller and SCP without an inverter, this would be the part that he wants.
Was this helpful?
What can we do to improve the information ?