Technical FAQs

Ask a Question

Ground Fault Fuse for Single Phase GT (NA models only), TX, MPPT60/80

Issue:

What is the ground fuse used in the Single Phase GT (NA models only), TX, MPPT60/80

Environment:

Single Phase GT (NA models only), TX, MPPT60/80

Resolution:

WARNING!!! SHOCK HAZARD !!! RISK OF INJURY!!! Do not replace the ground fault fuse without first verifying that the ground fault condition has been corrected. Ground faults must be diagnosed by qualified personnel. Always use an insulated fuse puller to remove / install fuses 

Fuse Rating: 1A, 600V(AC/DC), 100kA interrupt, Fast Acting, 5AG 1.50" x 0.406"
Fuse Model: Littelfuse KLKD001 or equivalent

The fuse is available at most industrial electrical suppliers or online from www.mouser.com  or www.newark.com or www.digikey.com   Schneider / Xantrex does not sell fuses. Fuses are not covered under the product warranty.    

Cause:

Ground fault fuse opened
Was this helpful?
What can we do to improve the information ?