Technical FAQs

Ask a Question

Gateway - Some Antivirus software blocks some Gateway communication

Xantrex has noticed that the antivirus program Bitdefender blocks certain communication from the Widget  via Wiport to the Gateway.  This may also be an issue with other antivirus programs.

 

 

 

The symptoms that may be noticed are:

 

1. The widget displays all the devices on the network but the detail screen does not display. 

 

2. The configuration pages appears to load up from cache but it does not display  build information in the upgrade tab. 

 

3. The time does not display in Time configuration tab.

 

4. IP addresses are not displayed in network configuration tab. 

Was this helpful?
What can we do to improve the information ?