Technical FAQs

Ask a Question

Low measured AC output on TR inverters

Under no load conditions, the voltage on the AC output will be ~104
for power savings or ~207 Vac under no load conditions for power savings for
230 vac/60Hz models. (Non-true RMS meters probably will not measure

To properly test inverter output, ensure that the batteries are appropriately charged, search mode is defeated, connect a load to the output of the inverter and test with a True RMS meter.

Was this helpful?
What can we do to improve the information ?