Technical FAQs

Ask a Question

Ferrite Rings for XW4548

The XW4548 (865-1005) is the only XW that ships with the ferrite rings. It also ships with an addendum to describe how to install them. The addendum number is 976-0185-01-01 and attached here for reference.

 The ferrite rings are there to reduce noise emissions at a very specific frequency. At 41MHz these ferrites reduce the radiated noise by about 6 [dB*uV]. Other than this frequency they do not have any other impact in emissions or unit functionality.
Was this helpful?
What can we do to improve the information ?