Technical FAQs

Ask a Question

XW Restore Defaults.

There have been isolated incidents of anomalies with the XW Inverter/Charger and the MPPT where "RESTORE DEFAULTS" will correct the symptom. It is usually related to Xanbus issues, i.e. only one inverter being displayed on the screen in a dual inverter system. There was even a case where the MPPT showed as being in BULK mode on the SCP, but no power out. Restoring to defaults corrected the symptom.
Was this helpful?
What can we do to improve the information ?