Technical FAQs

Ask a Question

Cannot log into Wireless Gateway even though IP address detected / discovered

Problem:

 Cannot log into Wireless Gateway even though IP address detected / discovered

 Environment:

 All computer OS'. All web browsers.

 Fix:

 Remove and re-seat the wireless board.

 steps:

1) remove the screw near the green connector 
2) push down on the tab above the antenna, and ease the board out 
3) re-insert board, ensuring the card edge connector inserts into the card slot solidly.
 
Was this helpful?
What can we do to improve the information ?