Technical FAQs

Ask a Question

GT CONFIG LITE Tech Instructions

 AC Voltage Fault will occur when the grid voltage varies outside of the inverter's anti-islanding range. This is usually more common when 2 or more inverters share the same lines or if there is heavy loading on the grid.

 

 

 

The Anti-Islanding settings can be re-configured. You will require the permission of the utility company before you open the anti islanding settings of the inverter.

 

 

 

Please see attached Software and User Guides

 

 

 

You will also need a Serial/USB cable and the dedicated driver it came with. Follow the instructions to get the cable working. Please see attached "GT RS232-USB Comm Info" as a good example.

 

 

 

Please review the GT Config Lite User's Guide for detailed info.

 

 

 

Here are the key points.

 

1. Install software / password is : xanadu (lower case)

 

2. VERIFY that you have POWER-OFF the GT

 

3. Connect the Serial/USB cable from the GT to your PC and also PUSH ONCE on the "PIC Enable Switch"

 

4. Now, POWER-ON the GT : Inverter will flash "EXT SHUTDOWN"

 

6. From here on, Refer to the GT Config Lite User's Guide, page 7-10 for image illustration

 

5. When changing a parameter, double click the desired cell in the ?WRITE? column and make the change

 

6. Click ?PROGRAM? to update and verify the change in the ?READ? column

 

7a. For UL-01, 864-0XXX inverters, you will be changing the High Threshold Phase to Phase and the Reconnect Voltage

 

7b. For UL-05, 864-1XXX inverters, you will be changing the High Threshold Phase to Neutral and the Reconnect Voltage

 

8. Now, VERIFY that you have POWER-OFF the GT , followed by release the "PIC Enable Switch" and remove your cable

 

9. Finally, POWER-ON the inverter

 

10. Check operation status

 

 

Was this helpful?
What can we do to improve the information ?