Technical FAQs

Ask a Question

Schneider Power meters for REC/FIT systems which meet ANSI C12.1-2008

Issue:
 
Some jurisdictions require grid tied inverters to have a revenue grade meter which meets the requirements of ANSI C12.1-2008. The meter in the single phase GT and XW do not meet these requirements

Environment:
 

Grid tied installations with a REC or FIT program in certain jurisdictions requiring meters which meet ANSI C12.1-2008

Resolution:
 

The following Schneider / PowerLogic power meters are listed in the CEC website as being eligible for use:

ION 6200,7330, 7350, 7550, 7650, 8600

Cause:

 ANSI C12.1-2008
Was this helpful?
What can we do to improve the information ?