Technical FAQs

Ask a Question

XW sell setup checklist w/MPPT 60/80.

Issue:

Checklist for setting up an XW system for sell. See XW operation manual for full full details.

Environment:
 
XW 4024 or XW 4548 or XW 6048 with f/w revisions 1.05 and above. MPPT60 or 80 charge controller. SCP 

Resolution:

1) Enable Grid support in XW setup menu
2) Set Grid support voltage to 64V and enable SELL in XW advanced - grid support menu
3) Verify CHARGE CYCLE is '2stgnofloat' in XW advanced - charger settings - charge cycle (factory default setting)
4) On MPPT set CHARGE CYCLE to '3 stage' in MPPT advanced - charger settings - charge cycle 
5) Is also recomended that the system has 100Ah for every KW of power that the customer wants to sell

Cause:

n/a
Was this helpful?
What can we do to improve the information ?