Technical FAQs

Ask a Question

How do I understand the positive and negative values I see on my XW SCP ?

Issue:

How do I understand the negative or positive Amp values I see on my XW SCP "SYSTEM STATUS" and XW Inverter-Charger "HOME"screens ?

Environment:

XW Systems and XW SCP Terminal

Resolution:

1. Battery Line
Charging Batteries - positive current value, in Amps (think of it as saving into your bank !)
Inverting / Selling (static mode) - negative current value, in Amps (think of it as withdrawal from your bank !)

2. AC1 line
Charging Batteries - negative current value, in Amps (think of it withdrawal from the utility !)
Selling - positive current value, in Amps (think of it as saving to the grid to make $)

In the Meters Menu (Refer to point 2)
AC1 Line 1
AC1 Line 2

Example
if AC1 L1 and L2 are negative Amp values, it means you are charging batteries




Cause:

NA
Was this helpful?
What can we do to improve the information ?