Technical FAQs

Ask a Question

XW Manufacturing

Lately, I have been getting a lot of questions of where the XW and XW components are made. So.... Here is the answer.


 


XW inverter chargers  - China
XW charge controllers - China
XW power distribution Panel 865-1015 - USA
XW System control panel 865-1050 - China


XW AGS- China


 


As for internal surface mount components, PCB's.


 


In general, Peoples Republic of China. Sheet metal and the bare PCBs are manufactured in China which is most of the value of the unit. Some components  come from Europe or Latin America. A little bit from North America as well, but the majority of electronic components are manufactured in SE Asia.


 


We don't have detailed records for every component as suppliers can manufacture parts in multiple countries depending on which plant has capacity to build. (Per Rob S)


 


Thomas.

Was this helpful?
What can we do to improve the information ?