Technical FAQs

Ask a Question

Gateway Widget Icon - Grid vs. Generator

The Widget displays a generator icon (off-grid) by default. If the XW AGS is in the network, the icon will always display the generator. If there is no XW AGS in the network, you can access the Multi- Unit Config segment of the ADVANCED menu for the XW Inverter/Charger (using SCP) and under CONNECTIONS, you must change AC2 to NONE. This will allow the grid icon to remain displayed on the Widget. This parameter may also be accessed using XW Config in the BASIC CONFIGURATION segment for the XW Inverter/Charger.

AGS operation and AC2 qualification are not affected by changing AC2 to NONE.


Qualification on AC2 causes the Widget to display the generator icon.


Was this helpful?
What can we do to improve the information ?