Technical FAQs

Ask a Question

TR series / Bulk charge cycle

The TR will only resume a BULK charge if the battery voltage is <12.5VDC (<25VDC for 24V models), or if the ON/OFF button is cycled while in STANDBY mode. Even if there is an interruption in AC input voltage, once AC is restored the TR will not resume a BULK charge unless the battery voltage is < the aforementioned reference voltages.

Was this helpful?
What can we do to improve the information ?