Technical FAQs

Ask a Question

Enhanced grid support not working properly

Issue:
 
Inverter can sell in Fixed mode but in Enhanced mode cannot sell .

Environment:

Grid support and sell enable

Resolution:
 
By looking at home page of inverter and SCC at SCP, if more than 0.4V difference in battery voltage reported on SCP, may cause enhanced grid support feature to not work properly.
More than 0.4V difference reported by inverter and SCC may be caused by bad DC connection and undersized cable for SCC or inverter.


Cause:

DC cables and connections need to be verified .
Was this helpful?
What can we do to improve the information ?