Technical FAQs

Ask a Question

XW 3-PH Config

After 120V conversion, you MUST assign a device NUMBER other than "00" (default) in order to select between 1-PH Master/Slave or 3-PH Master/Slave options. Also, it is possible to configure 3-PH Masters using only (2) inverters (A and B), HOWEVER, the system will NOT transfer unless (3) inverters are in the system (Phases A, B, and C)
Was this helpful?
What can we do to improve the information ?