Technical FAQs

Ask a Question

Conext TX is discontinued

Issue:

Schneider Electric no longer offers a 1-ph solution for grid-tied inverters in North America.

Environment:

Client (End User) has GT single phase inverter that has failed out of warranty.



Resolution:

We offer a battery-based solution only. XW+NA has sell capability and provides backup. 
This model requires a 3rd party battery bank and at least one MPPT80-600 charge controller
(if array is to remain in same configuration as with GT). 
SCP or Combox required for programming.
http://solar.schneider-electric.com/product/conext-xw-na-solar-inverter/

If customer wants to replace with grid-tie, they will have to consult their installer for recommended replacement from another company (i.e. SMA or Fronius)




 

Cause:

Discontinued product offer.
Was this helpful?
What can we do to improve the information ?