Technical FAQs

Ask a Question

What are the Modbus registers on the Conext TL.

Issue:

What are the Modbus registers on the Conext TL

Environment:

Conext TL inverter

Resolution:

Please see the attached document

Cause:

The Conext TL inverters do not share the same modbus register map as the Xanbus-based inverters such as the XW, TX, and 1-ph GT.
Was this helpful?
What can we do to improve the information ?