Technical FAQs

Ask a Question

MPPT80 grounding

Issue:

If I ground my PV array positive by installing fuse in positive ground fuse holder, will my battery positve also grounded?

Environment:

XW system using SunPower solar panels

Resolution:

PV input and Battery output are isolated. The positive or negative of the battery can be grounded independent of the array grounding. This means you can ground battery negative while keeping the PV positve grounded.

Cause:

none
Was this helpful?
What can we do to improve the information ?