Technical FAQs

Ask a Question

Combox Modbus Support

Issue:

What kind of modbus support for Xanbus devices does the Combox offer?

Environment:

Conext Combox with any of the following:

 Conext SW
 XW Hybrid Inverter / Charger
 XW Automatic Generator Start
 XW MPPT 60 150
 Single-phase Grid-Tie/TX
 XW System Control Panel
 XW MPPT 80 600



Resolution:

- The combox supports a set of read/write commands to the above xanbus devices. These commands are attached in the document 'ComboxModbusMap.zip'. Some listed commands are for future use and are not currently implemented
- The combox offers Modbus support through RS-485 or Ethernet/TCP (port502)
- Note that the combox does not proxy modbus addresses like the Wireless Gateway. Xanbus devices can now be addressed directly
- Assigned modbus addresses for atttached supported xanbus devices are listed in the combox SETUP section - MODBUS ADDRESS LIST

Cause:

n/a
Was this helpful?
What can we do to improve the information ?