Technical FAQs

Ask a Question

AGS type connections

Issue:

 AGS displays warning W202 " Unable to start generator "

Environment:

AGS connections and Gen Type selection

Resolution:

Determine the action of the start switch.
      - After determining the sequence of actions that the generator requires to start choose the correct type.
      - Once the correct type has being selected then the generator should be able to start by selecting Manual ON.
      - If the generator does not:
               - Make sure that the connections for the relays are made (i.e. connections form the Bat - or common to the relays that are used to start the generator
               - Make sure that the generator is not a grid loss sense generator


Cause:

Setting up the AGS 
Was this helpful?
What can we do to improve the information ?