Technical FAQs

Ask a Question

TR Inverter/Charger F08

Issue:

TR displaying F08(Low Battery Wanrning)

Environment:

If the battery falls below a set value placed by the Overdischarge funciton of the unit, the inverter will display an F08

Resolution:

The Overdischarge Protection is automatically enabled on the inverter which is used to calculate a safe cutoff value for the battery based on the capacity and the load demand.
If an F08 occurs you can temporairly disable the ODP by pressing the ON/STANDBY switch, but you would need to check your batteries or reduce your load.

Cause:

At least one connected battery has dropped below the ODP threshold set.
Was this helpful?
What can we do to improve the information ?