Technical FAQs

Ask a Question

Conext SW - Installation/ Wiring issue

Issue:

Customer is installing the Conext SW and wants to confirm the wiring of the AC and DC cabling. 

Environment:

Conext SW 2524 120/240 Split-phase (865-2524)
 
Conext SW 4024 120/240 Split-phase (865-4024)


Resolution:
 

See the attached wiring diagrams for the Conext SW and Conext SW-NA.
Do not mix AC and DC wiring in the same conduit or panel. Consult the applicable installation code for details.
There are two dual 3/4" /1" trade-size knockouts on the side panel and another two on the bottom panel for AC wiring. Use the same trade size of strain relief as the trade size of the knockout(s) you are using.

 
Was this helpful?
What can we do to improve the information ?