Technical FAQs

Ask a Question

Conext Combox RS-485 modbus settings

Issue:

What are the default modbus / RS-485 settings in the Conext Combox

Environment:

Conext Combox

Resolution:

RS485 Serial Protocol: 19200, E, 8, 1
Modbus Mode: RTU
Modbus address (Combox): 201
Byte Order: LSB first

Cause:

n/a
Was this helpful?
What can we do to improve the information ?