Technical FAQs

Ask a Question

How do I access the ACTIVE POWER menu in the Conext TL?

Issue:

How do I access the ACTIVE POWER menu in the Conext TL?

Environment:

Conext TL series inverters

Resolution:

The Active Power menu can only be accessed if the COUNTRY is set to CUSTOM, Germany LVD/MVD or Italy BT **** AND THE SETTING IS SAVED *****

After the COUNTRY is seLECTED PRESS enter, then press ESC to save the country setting - you will be returned to the password menu. Enter password and hit ENTER. The active power menu should appear 

Cause:

Product design
Was this helpful?
What can we do to improve the information ?