Technical FAQs

Ask a Question

Conext SW Neutral Switching.

Conext SW Neutral Switching

Issue :
Conext SW series switches the NEUTRAL (disconnects from internal transformer) for AC pass thru (120/240V input). Neutral IN/OUT are common within the CSW, so having a completely isolated and separate NEUTRAL for input and output is unnecessary (diagram on pg.3-8 must be noted, which shows common NEUTRAL). 

Environment :
Residential Battery-Backup

Resolution :  
Be aware CSW has common neutral internally.

Cause :   
Conext SW neutral switches internally to energize transformer for split-phase when inverting, and when supplying 120VAC to L1-N. When operating as charger for 120/240VAC source, the internal neutral relay disconnects from transformer so it operates as stricly 240V charger.
 
Was this helpful?
What can we do to improve the information ?