Technical FAQs

Ask a Question

XW AGS Max Run Time


Customer wants generator to run longer than 8 hrs, but AGS faults due to Max Run Time


Commercial/Residential Backup


Set for Type14

New firmware allows Max Run Time to be set up to 24 hrs, or disabled (set to "0").
Since Type14 does not monitor a run signal, nor does it consider the presence of AC to determine the gen has started, it will read "Running" even when the gen is off. 
It will respond to Max Run Time by turning the generator off. 
Was this helpful?
What can we do to improve the information ?