Technical FAQs

Ask a Question

Do our energy efficient, low voltage, dry type transformers like EE45T3HCU meet NEMA 250 requirements ?

Issue:
Standards compliance

Product Line:
Low Voltage Distribution Transformers

Environment:
Energy Efficient type

Cause:
UL

Resolution:
Yes. This is an enclosure standard we meet and exceed by building to  UL1561

Was this helpful?
What can we do to improve the information ?