Technical FAQs

Ask a Question

Do the ATV61 drives meet the US standard Nema ICS-61800?

Issue:
Do the ATV61 drives meet the US standard Nema ICS-61800? They understands that it meets European IEC-61800 standards.

Product Line:
Altivar ATV61

Environment:
All

Cause:
They are trying to understand the drives standards.

Resolution:
Because ICS 61800 refers to IEC 61800, we can say that we conform but we have no document for ICS.
If it's for a big market, we can contact the product manager for further assistance.
Was this helpful?
What can we do to improve the information ?