Technical FAQs

Ask a Question

If I add an additional System Control Panel to my network having one already, will the settings update to match the original inverter?

 Installing two System Control Panels in the same xanbus network

If you wish to incorporate an additional system control panel, the setting will automatically update to the ones set up for the original system control panel.
Reason: Settings are stored in device's non-volatile memory and broadcast to the SCP

NOTE:  The following test was done in our lab and confirmed to do just that. Tested with latest firmware on SCP (1.6BN19)
Was this helpful?
What can we do to improve the information ?