Technical FAQs

Ask a Question

What is the replacement for a MHL3630025DC3903

Product Line:
MH DC Breakers

Resolution:
This item is OEM part that was purchased under the number 519568P14.
It is a 300A 3 pole 500 Vdc breaker with (1284) 1A/1B gold flashed auxiliary contact, and a (3900) 48VDC Under Voltage Release, with 48 inch leads.
The  replacement is LGL37030D27AEUP; must be built in product selector.


 
Was this helpful?
What can we do to improve the information ?