Technical FAQs

Ask a Question

Can the ATV61 drive provide 150% of the motor current for 3 seconds on the 250HP to 700HP drives?

Issue:
Exceed motor current.

Product Line:
ATV61

Environment:
ATV61HC50N4
ATV61HC40N4
ATV61HC31N4
ATV61HC25N4
ATV61HC22N4
ATV61HC16N4

Cause:
Can the ATV61 drive provide 150% of the motor current for 3 seconds on the 250HP to 700HP drives?

Resolution:
It is not possible to provide 150% of the motor current for 3 seconds on the drives listed.  However if the drive is oversized by one size it is possible.  It is recommended to use the ATV71 of the same rating. 
 

Was this helpful?
What can we do to improve the information ?