Technical FAQs

Ask a Question

Are two EK200DTU2 required for use on the C82344, Canadian 200A Double Throw Switch?

Issue:
Selection

Product Line:
Double Throw Safety Switch

Environment:
Electrical Interlock Accessories

Cause:
Selection criterea

Resolution:
Only one kit is required. The kit will provide 2NO/2NC auxiliary contacts for each of the two operating positions. 

Was this helpful?
What can we do to improve the information ?