Technical FAQs

Ask a Question

Can I get an E-flex system with the keypad mounted on the outside of the cabinet door?

Issue:
ECan I get an E-flex system with the keypad mounted on the outside of the cabinet door?

Product Line:
8839EFD E-flex enclosed ATV61 drive systems.

Environment:
NEMA 1 or NEMA 12K enclosed only, All serial numbers.

Issue:
Customer wants to be able to monitor the keypad and make adjustments without stopping the drive and opening the cabinet door.

Resolution:

The NEMA 1 and NEMA 12K enclosed E-flex systems have this option available.  Under "Control Options" section of the part number, select any option other than N07 (No operators) will include a graphic keypad (VW3A1101) mounted on the cabinet door.  The NEMA 3R version of the E-flex is not available with the keypad mounted on the cabinet door.
Was this helpful?
What can we do to improve the information ?