Technical FAQs

Ask a Question

Is a pneumatic unloader for Schneider Electric disconnects

Available in NEMA line only (customer looking for IEC version)

Issue:
Pneumatic unloader for IEC disconnect

Product Line:
Vario, LK4, GS2/3

Environment:
US product

Cause:
Needing pneumatic unlaoder valve for compressor to be used in conjunction with disconnect

Resolution:
Unloader valves are not available as accessories for IEC style devices.  They are available with 9422 NEMA disconnects, and are part numbers 9422G1 and 9422G2

 

 
Was this helpful?
What can we do to improve the information ?