Technical FAQs

Ask a Question

Can I use a C-series or MPPT on a Mobile Application?

 Using a C-series on a Mobile Application

 

Issue:

Solar Charge Controller Needed on a Mobile Application

Resolution:

The C-series controller is approved for UL1741, which applies to residential installations.  The C-series has a metallic chassis that must be earth-grounded with a ground rod.
Unfortunately, Schneider-Electric does not make a Solar Charge Controller that is approved for Mobile applications.
Neither the C-Series nor the MPPT series manufactured by Schneider Electric are UL-458 certified. 

Was this helpful?
What can we do to improve the information ?