Technical FAQs

Ask a Question

Where can I find the GTI so that I can allow my TRACE SW to sell power back to the utility?

 TRACE GTI

Issue:

Setting a TRACE SW inverter to be able to sell power back to the grid

Resolution:

The GTI is an accessory for the Trace SW inverters that provide the unit with anti-islanding capability, and is designed for use with Trace SW models with 4.2 or newer software (DOM 2001). The GTI is required for the inverter to be able to be compliant with the NEC code of North America. The following link is a distributor that still offers this product. :

 

TRACE GTI:

 www.solarelectricsupply.com/Inverters/xantrex/gti.html

TRACE GTI Manual:

Was this helpful?
What can we do to improve the information ?