Technical FAQs

Ask a Question

Can I have more than One SCP on the XW or SW system?

 Multiple SCP on the XW or SW system
Issue:
Multiple SCP
Resolution:
The XW and the SW systems can handle more than one SCP. However, you should always keep in mind the limitations of Xanbus communication. See article FA229214 and FA229325. 
Only one SCP will be displayed in respective "Select Device" list.
 
Related Product:
SCP
Was this helpful?
What can we do to improve the information ?