Technical FAQs

Ask a Question

How is a preset speed programmed in an ATV31 or ATV312 drives?

Issue:
How is a preset speed programmed in an ATV31 or ATV312 drive?

Product Line:
ATV31 or ATV312

Environment:
All

Cause:
Logic input to trigger a preset speed LIX

Resolution:
In the Application Function Menu (FUn-), select the Preset Speed submenu (PSS-).
Set PS2 to the logic input that will activate the preset speed.
Set PS4 to the logic input that will activate the preset speed.
Set SP2 to the desired speed in Hz.
Set SP4 to the desired speed in Hz.
Was this helpful?
What can we do to improve the information ?