Technical FAQs

Ask a Question

Is there an enclosure still available for the obsolete MAL or MHL circuit breakers?

Issue:
Enclosure availability

Product Line:
Circuit Breaker Enclosure

Environment:
All NEMA Types

Cause:
Enclosure for an obsolete circuit breaker

Resolution:
All circuit breaker enclosures for the obsolete MAL or MHL circuit breakers are also obsolete and no longer available. Consider using a PowerPact M-frame circuit breaker (800A max) or PowerPact P-frame circuit breaker (1200A max).
Was this helpful?
What can we do to improve the information ?