Technical FAQs

Ask a Question

What's included in form M10 marine control adder for Size 1 thru 6 starters, contactors and Duplex panels?

Issue:

What is included with form M10?

Product Line:
Nema Starters, Contactors and Pump panels

Cause:
Customer needs to verify what modifications are made for Form M10

Resoluion:
Following modifications are made to make devices more condusive to salt water applications:
Nameplate is made from Non Corrosive material , Seals material is changed and coating is modified.

Keywords: 8502, 8536, 8538, 8539,8736, 8738, 8739, 8810 8941

Was this helpful?
What can we do to improve the information ?