Technical FAQs

Ask a Question

Form M10 for Size 1 - Size 6 Starters

What is included with form M10 (Marine standard)  for Nema starters, contactors and duplex controllers?

Product Line:
Nema Starters, Contactors and Pump panels

Marine rating for Nema starters, contactors and duplex controllers. 
Customer needs to verify what modifications are made for Form M10

Following modifications are made to make devices:  more condusive to salt water applications:
Nameplate is made from Non Corrosive material , Seals material is changed and coating is modified.
This applies to Nema 4 or 12 devices for use as Marine control per UL508 Marine supplent SA)


Was this helpful?
What can we do to improve the information ?