Technical FAQs

Ask a Question

Is HU661DS CSA Certified?

Issue:
Standards

Product Line:
Heavy Duty Safety Switch

Environment:
6 pole non fused safety switch

Cause:
Assurance of standards met

Resolution:
Yes, HU661DS is CSA Certified as well as UL Listed. Both CSA and UL marks are applied to the wiring diagram.
Was this helpful?
What can we do to improve the information ?