Technical FAQs

Ask a Question

How do I connect the Kohler RES generators to the AGS

 

 Kohler RES remote start wiring to the AGS

Kohler RES generators have a remote port located on the back side of the unit labeled Slot 3 and Slot 4. This is not a simple on/off setup. It actually requires a voltage signal to have the unit operate. The slot 3 is going to be the crank motor for the generator. Slot 4 of the generator is going to be the RUN/Stop signal for the unit. Here is a wiring schematic to connect the Kohler generator to the XW AGS. Please note that the Batt+ is connected as a common wire between XW AGS's wires 16 and 18; these connections are not made internally and must be done in order to have the system operational.
WARNING : NO RUN SIGNAL REQUIRED. IN FACT, RUNNING A JUMPER FROM 16 to 13 AS OUTLINED IN THE MANUAL WILL CREATE DEAD SHORT, AS RELAYS ARE ACTIVE HIGH IN THE ATTACHED DIAGRAM!
See attached.




Was this helpful?
What can we do to improve the information ?