Technical FAQs

Ask a Question

A Masterpact NW opens slowly while the spring is being charged with the handle.

Product Line:
Masterpact NW

There is an internal problem with the breaker mechanism causing it to slow-open.  This cannot be repaired, so the breaker must be replaced.
Was this helpful?
What can we do to improve the information ?