Technical FAQs

Ask a Question

What is the difference between an EIK032 and an EIK034M Electrical Interlock Kit?

Issue:
Application

Product Line:
Heavy Duty Safety Switch

Environment:
Application

Cause:
Selection

Resolution:
Both of these Electrical Interlock Kits provide 2-NO/2-NC auxiliary contacts, however they use different limit switches to provide the contacts. The EIK032 contain one 9007CO3 limit switch manufactured by Schneider Electric. The EIK034M contains two 3MN1 limit switches manufactured by Micro Switch. The instruction bulletins for both devices are provided below.
Was this helpful?
What can we do to improve the information ?