Technical FAQs

Ask a Question

What are the repair parts for the H361DX, Series F01 (may be shown as Series F1)?

Issue:
Repair parts

Product Line:
Heavy Duty Safety Switch

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Repair parts for the H361DX, Series F01 are as follows. No other parts are available.
-Interior Assembly - 9422TCF33 (includes the line and load base, mechanism and operating rod)
-Handle Assembly - NF200
-Enclosure Mounting Foot - 0201847 (4 total required)



CTA-ID : 2005144
Was this helpful?
What can we do to improve the information ?